3/4/2012 4:42 PM | |||||||||||||||||||||||||||||||||||||
Joined: 1/12/2012 Last visit: 12/25/2023 Posts: 22 Rating: (0) |
We have one defected synchronization sub-module with part number “6ES7960-1AA00-0XA0” when we issue to purchase another one. We found that our part number is being cancelled by Siemens and substituted by part number “6ES7960-1AA04-0XA0”. So, please advise us with the scope of compatibility for the new synchronization sub-module with our existing system. Table below show our existing system:
|
||||||||||||||||||||||||||||||||||||
3/9/2012 2:25 PM | |
Posts: 27 Rating: (1) |
Hi The Sync modules and Sync cables are new and therefore not compatible with the previous ones. In view of the fact that H systes always require two CPUs with the same hardware and the same firmware, both CPUs, the Sync modules and the Sync cables would have to be replaced. This will only be practicable in exceptional cases. For this reason the CPUs and Sync components will remain available on a spare part basis. ...so it is written here: http://support.automation.siemens.com/WW/view/en/21790608 So ask by Siemens to "change" your def. modul. |
4/23/2012 4:30 PM | |
Posts: 947 Rating: (45) |
for older CPU and sync modul number CPU in rack was at sync modul, for new - on back side CPU |
4/23/2012 5:35 PM | |
Posts: 23 Rating: (3) |
Dear mohamed s gaber, As in your first link, click on "Spare Part investigation" and order a spare part. |
Follow us on