11/26/2021 9:45 AM | |
Joined: 11/4/2011 Last visit: 7/19/2024 Posts: 229 Rating:
|
Just have a look at the technical data: https://support.industry.siemens.com/cs/de/en/pv/6ES7516-3TN00-0AB0/td?dl=de Section "Supported technology objects" contains all the information you need. There you can see how many motion credits the PLC offers, and how many are used per TO (depending on the type). So this is the maximum amount in regards to memory. The other point is the performance. This is pretty hard to say, best you check with TIA Selection Tool, this provides information about the possible timings, taking the amount of TOs into consideration. Regards, |
Follow us on