11/21/2012 3:28 PM | |
Joined: 7/7/2010 Last visit: 2/12/2025 Posts: 15630 Rating:
|
I agree with Ganes10there should be a better way with the NEW software that is at least as good as the OLD software. A couple of approaches, one already mentioned, would be something like this: Have one project with 2 PLCs and 2 HMIs, and just change the IP address to match which device you are loading. Have one project with 6 PLCs and 6 HMIs, and just update the top 2 PLCs/HMIs, then drag / drop any updates to the remaining PLCs/HMIs. This is more work, more error prone, but does allow for future customization to each PLC/HMI should the need arise. |
science guy |
|
This contribution was helpful to
1 thankful Users |
Follow us on