8/16/2017 7:25 AM | |
Joined: 3/1/2016 Last visit: 5/21/2024 Posts: 6 Rating: (0) |
Using a Simatic field PG M3 (6ES7 715-1BB20-0AE1) and a S5 cable (6ES5 734-2BF00) I try to establish a connection with Step5 V7.23 under Windows XP SP3 and a S5-100U (CPU102) PLC but I get the error message: "System message no. 0317". The S5@@@@AS.INI file is like: [COM1:] Could someone help me? Edit (2017.08.17): Is there any other cable to be used? Attachmentscreenshots.zip (412 Downloads) |
Last edited by: M_Franke at: 8/17/2017 6:55:28 AM |
|
Follow us on