3/9/2015 8:32 AM | |
Joined: 3/9/2015 Last visit: 3/8/2024 Posts: 2 Rating: (0) |
Hi The User use 6RA70 and T400. See attachment, the user sent to me the program.Use D7 SYS 8.0. When compilation its is giving the error. “SDE-LD exits with error.” Please suggest me for solution . Attachmentbc1fs20140328.rar (196 Downloads) |
Last edited by: AutoGen_913971 at: 3/9/2015 8:51:55 AM |
|
3/10/2015 6:38 AM | |
Joined: 3/9/2015 Last visit: 3/8/2024 Posts: 2 Rating: (0) |
I have reinstalled again.but also give the same error. Is there something wrong with the system version? |
3/10/2015 7:03 AM | |
Joined: 8/25/2006 Last visit: 5/3/2024 Posts: 2203 Rating: (277)
|
Hello. Win7 Enterprise is not compatible with CFC V8.0 and D7-SYS V8.0. It can be used only with Step 7 from V5.5 SP1. For Step 7 + CFC + D7-SYS you need Win7 Professional or Ultimate, check here. |