7/14/2011 6:05 AM | |
Posts: 47 Rating: (0) |
Dear Expert I tried to download CFC program fornew T400 (6DD1606-0AD1), the download process ran to 100% then I got fault messageas attached file here. I already tried to recompile HW, CFC program(no fault) and downloaded again but got the same fault. I go to HW configure and could not see 6DD1606-0AD1 (only see6DD1606-0AD0). Itry to look for new firmware butI could notse any firmware or GSD file for 6DD1606-0AD1. I also update newhardware but problem are the same (no 6DD1606-0AD1). Could you please give me solution how to solve my trouble and doI need to use 6DD1606-0AD1hardware to download to new T400 card? Thank you very much Best regards Sie-auto AttachmentT400 Falut.zip (400 Downloads) |
7/14/2011 11:50 AM | |
Posts: 47 Rating: (0) |
Dear Mr. KSN and others When I download program to T400, I got fault message error 4305 then drive fault F080. I already tried to turn on/off power, replaced a new one but the fault was the same. ifI push back the old one (this is T400 in good for runningbutI take out of drivefor test a new T400) so drivecan run, no fault. I attached here a zip file as T400 CFC program and drive parameters, please have look and give me solution how to sole the problem Thank you very much AttachmentDesktop.zip (376 Downloads) |
7/19/2011 5:05 PM | |
Posts: 47 Rating: (0) |
Dear Sir Could you tell me how can I get it. if you need firm ware, pls go to http://support.automation.siemens.com/WW/view/en/10804947/133100 Thank you very much Best regards sie-auto |
Last edited by: sie-enauto at: 7/19/2011 5:33 PM |
|
7/19/2011 5:32 PM | |
Joined: 8/25/2006 Last visit: 10/18/2024 Posts: 2209 Rating: (279)
|
Hello. May be this is what you are looking for: MASTERDRIVES VC, compact-/chassis, firmware V3.41 MASTERDRIVES VC, compact-/chassis, hotfix for firmware V3.42, 4 languages + italian. |
Last edited by: KSN at: 7/19/2011 5:35 PM |
|
Follow us on