6/10/2008 1:02 PM | |
Posts: 1776 Rating: (95)
|
Hi, if you have an integrated project, you can use the "OS transfer" function. detailed informations are given in the online help |
6/10/2008 1:55 PM | |
Joined: 12/8/2006 Last visit: 11/27/2023 Posts: 170 Rating: (26) |
hi, if you don't have an integrated wincc project you have the following opportunities to create tag logging archives: ========================== 1) using default tag logging editor ========================== the editor wincc tag logging doesn't support bulk operation, BUT: -Adapt the pre-Setting for an archive tag before you create the archive tags!!!!!! "Tag Logging > Archives > Pre-Settings > Analog Tag" - you can create multiply archive tagsby one operation if you select more than one tag in creation dialog http://support.automation.siemens.com/WW/view/en/24193860 ========================== 2) Excel-Based configuration ========================== - WinCC Smart tool "Configuration Tool" - WinCC Smart tool "Archive Configuration Tool" (==> select smart tools during wincc setup) |
Follow us on