12/23/2015 1:06 PM | |
Posts: 79 Rating: (9) |
Hi, I am working on that at the moment... I found a very good example project whitch show how to read the tags archive. You have to install the WinCC Connectivity Pack to be able to do that. Since WinCC 7 (not sure), all the values are compressed. It's impossible to see the values directly in the database slow like with WinCC6.2... Here you have other tools, but I didn't succeed with it.. Regards |
12/23/2015 1:19 PM | |
Posts: 22 Rating: (0) |
Thanks, but I don't need to read the tags. I need configure "compressed archives" and manage files backup with being sure to be able to view the data through the TrendControl next year with standart Export to CSV ability. "Data for each second stored in compressed form" and "making up the separated table of average values for each timing group (an hour)" - these are different things. I need information about managing the "compressed archives" as they are. |