6/16/2016 11:25 AM | |
Joined: 6/3/2014 Last visit: 1/17/2023 Posts: 660 Rating:
|
Hello Derek M, did your tags start to show 0 suddenly during runtime or during the engineering process (new start of the runtime for testing)? Did you delete the tags in the PLC tag table/DB or the HMI tag table? To add the tags to a new screen you could connect to the tag in the PLC directly. You say the values on the screen show again. So if you look to which tag the I/O field is connected, the missing tag is still displayed there, just not in the HMI tag table, yes? I have two suggestions for you:
|
~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ★ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ |
|
This contribution was helpful to
1 thankful Users |
Follow us on