3/8/2023 2:07 PM | |
Joined: 5/16/2020 Last visit: 7/16/2024 Posts: 4 Rating: (0) |
I have the same problem with WINCC UNIFIED 18 , tags are read without problems , but can't write in any way (Textbox / Script etc ... this happens with Bool , Integers from PC simulation and from Phisical HMI Panel) The DB is ok (i check the same variables with a NOT Unified panel and works) so the problem is only for UNIFIED panels. During test i have found a strange behavior of monitoring of DB if i try to modify current value of one variable is opened yhe popup with random values ... i don't know if is related to this problem or is one general problem o Version 18 .... ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 03/09/2023 07:52:04New subject after splitting |
|
6/27/2023 7:40 AM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8175 Rating: (173) |
New question published by AutoGen_5568354 is split to a separate thread with the subject Tags cannot write in any way and fonts do not match those set in the project.. Best regards |
Follow us on