11/7/2018 1:39 PM | |
Joined: 4/28/2015 Last visit: 4/30/2024 Posts: 3345 Rating: (377)
|
Hi, which option do you want to use? One possibility is to build an image on your own with the latest tar included. Another one is to install the latest tar from source on the IOT. This is the gnu tar. Copy the downloaded tar.xz file to your IOT and extract it with
Then go to the extracted folder and type in
that command is for configuring the package as root. Then type in
then
and then
I am trying this right now, but this takes a long time.. I will inform you when it is done. ------------------------------------- Best regards! |
Last edited by: bergmanu at: 11/7/2018 2:09:50 PMLast edited by: bergmanu at: 11/7/2018 2:22:53 PMadded screenshot after test Not working for IOT2050 support anymore from March 1st, 2024. |
|
This contribution was helpful to1 thankful Users |
Follow us on