12/19/2018 2:34 PM | |
Joined: 8/3/2009 Last visit: 5/10/2024 Posts: 12924 Rating: (1646) |
Hello Here are the general Information: https://support.industry.siemens.com/cs/ww/en/view/20982954 Bye Murof |
If this Information really helps, you could use the Rate function |
|
1/8/2019 3:52 PM | |
Posts: 5 Rating: (1) |
Hello again, I started to use AG_SEND and AG_RECV. When configuring the NetPro how should I configure my third party controller? I found quite useful information in the following link. However, they use there two S7 devices, one for sending and the other for receiving. In my application it's just one PLC which is used for both sending and receiving commands to a controller. https://support.industry.siemens.com/cs/ww/en/view/8707570 How could I adapt the instructions for my convenience?? Thank you very much Álvaro |
Last edited by: Jen_Moderator at: 1/9/2019 12:42:15 PMOptimized link. |
|
1/9/2019 9:56 AM | |
Posts: 5 Rating: (1) |
Hello Kaulquappe, Thanks for your answer. Still I'm little *** for using TCP/IP communications in Siemens. Have you taken a look to the link I sent you? Could it be used as a guide for my application? These two links I think they can be helpful for my programm, can you confirm it or would you recommend me any other guide? https://support.industry.siemens.com/cs/ww/en/view/8707570 https://support.industry.siemens.com/cs/ww/en/view/18843927 Thank you very much, Álvaro |
Last edited by: Jen_Moderator at: 1/9/2019 12:43:16 PMOptimized links. |
|
1/9/2019 2:25 PM | |
Posts: 3093 Rating: (322)
|
Hello, Regards, |
Follow us on