4/9/2013 7:04 PM | |
Joined: 7/7/2010 Last visit: 5/17/2024 Posts: 14751 Rating: (2373) |
Can you configure the drive for PZD 8/8? If so, you can possibly ask Siemens for a GSDML file that supports profinet 8/8. I used an xml editor to create a simplified version of the GSDML file (english only) that added telegram 999 with 8/8. Whether it would work for your application is unknown. I post it here in the event you find it a useful concept. As an FYI, this may not work, but then again, it might work. Since it is not provided by Siemens, it may cause problems as they understand the requirements. However, it did add to my project and show PZD 8/8 which should match up with a CU240S PN if it is configured for 8/8 as well. My guess is this uploaded customized GSDML might not be appreciated, so get it, look at what was changed, and decide whether to use support request or perhaps modify your own custom gsdml file as your needs dictate. I have a running application with a custom GSD file and it works very well for our needs. The vendor provided the specs for customizing the gsd file. Post your thoughts and results. AttachmentC:\TEMP\GSD\GSDML-V2.0-custom-sinamicsg120-20130409.zip (382 Downloads) |
science guy |
|
This contribution was helpful to2 thankful Users |