9/13/2021 4:34 AM | |
Joined: 12/18/2014 Last visit: 5/15/2024 Posts: 33042 Rating: (4082)
|
Thank you, you are too gracious ... |
9/13/2021 7:34 AM | |
Joined: 12/18/2014 Last visit: 5/15/2024 Posts: 33042 Rating: (4082)
|
Here's a possible solution (TIA V13 SP2 Upd4 and LOGO! 0BA8.Standard). The setpoint setting is limited to 40,0 °C at maximun and 20,0 °C at minimum. A start value is set by 30,0 °C, Attachmentperhvid.zip (398 Downloads) |
9/13/2021 8:04 AM | |
Joined: 5/25/2020 Last visit: 3/16/2024 Posts: 32 Rating: (0) |
thanks for the program I had never even come up with. may I get a password so I can try it out in my logo |
9/13/2021 8:21 AM | |
Joined: 5/25/2020 Last visit: 3/16/2024 Posts: 32 Rating: (0) |
when I try to download two logo. I've never seen that with my own programs |
9/13/2021 7:57 PM | |
Joined: 5/25/2020 Last visit: 3/16/2024 Posts: 32 Rating: (0) |
sorry i did not try it better off. it seems perfect. many thanks for the help. |
Follow us on