3/10/2010 4:15 PM | |
Posts: 131 Rating: (0) |
Dear all, how is the best way to test the IGBT inside a Simovert Masterdrive? i.e. to see if it must be replaced or not. |
3/10/2010 11:12 PM | |
Joined: 6/4/2008 Last visit: 6/27/2024 Posts: 1485 Rating: (323) |
The ideal way to test an IGBT is to run it under load, however, it is possible to test it at 24VDC. Using the Masterdrive testbox is one way (6SE7090-0XX84-1FK0) Please see the attached documents for testing IGBT's and SCR's (Rectifiers) with meters, maybe they can help you. Cheers, Graeme AttachmentIGBT_&_SCR_Testing.zip (2112 Downloads) |
This contribution was helpful to5 thankful Users |
7/19/2011 6:25 PM | |
Posts: 1 Rating: (0) |
Pleasse tell me how can i test IGBT & SCR by using mutimeter |
4/30/2014 10:20 PM | |
Posts: 4 Rating: (0) |
thanks for your guidance.its very useful. |
This contribution was helpful to1 thankful Users |
Follow us on