11/24/2011 1:25 PM | |
Joined: 10/26/2011 Last visit: 12/2/2024 Posts: 762 Rating: (192) |
Hello dzwilu, the block comment is only in single language. For additional languages you have to change the block comments in the text library. Regards |
SIMATIC PCS 7 - Overview |
|
11/25/2011 1:24 PM | |
Joined: 10/26/2011 Last visit: 12/2/2024 Posts: 762 Rating: (192) |
Hi What is your default language in the SIMATIC Manager (menue "Option >Language for Display Devices")and in WinCC? English oder Polish? In which language did you change the comments? If you change the comments in the CFC-Chart and compile, then the Mapper looks in the text library. If the text is not available in the default language, it adds a new row with the new comment. Regards |
SIMATIC PCS 7 - Overview |
|
11/30/2011 2:43 PM | |
Joined: 10/26/2011 Last visit: 12/2/2024 Posts: 762 Rating: (192) |
Hello dzwilu I think too, that the different language engineered CFCs are the problem. I am not sure, if the following abstract can help you: Abstract: "Options > Manage Multilingual Texts > Change Languages..." menu After the text types of the project have been translated and imported, you can use this dialog field to select the language in which to display these text types. You can select whether the language is changed for title and comments or display texts or both. This language change is object related, i.e. you can trigger a language change separately for projects, stations, programmable modules, S7/M7 programs, symbol tables, block folders and all blocks. The languages which are available in this context depend on the selection under "Options > Language for Display Devices". All languages installed in the project can be selected here. Note The language change for "Title and comments" is only executed for the selected object. The language change for "Display texts" always causes a language change in the entire project. |
SIMATIC PCS 7 - Overview |
|
12/8/2011 10:06 AM | |
Joined: 10/26/2011 Last visit: 12/2/2024 Posts: 762 Rating: (192) |
Hello Dzwilu |
SIMATIC PCS 7 - Overview |
|
12/8/2011 2:15 PM | |
Joined: 10/26/2011 Last visit: 12/2/2024 Posts: 762 Rating: (192) |
Hello Dzwilu I hope you will find the problem in the documentation or you will get a tipp there. At the moment I have no moreideas, where you can look or what you can do. I think, you check the sub-folder via this way: Mark the the sub-folder menu bar > options > Manage Multilingual Texts > Change Language" The displayed language is the set language. Are the cehck boxes of "Title and Comments" and "Text Display" activated? Regards |
SIMATIC PCS 7 - Overview |
|
Follow us on