8/23/2017 3:27 AM | |
Joined: 8/22/2013 Last visit: 6/5/2021 Posts: 62 Rating: (0) |
Dear all, Now our machine i have a problem. The encoder connection through the slip ring. But when the fault happen,the machine is still ok, but when we reset the fault, the machine emergency stop, why? In the attachment how do you think the alarm ,is the reason of not good connection or EMC? And in the attachment "help for event" what does "Acknowledge : pulse inhibit" mean? I think the fault (no.31115) will acknowledge automatic, is that right? And what does the"pulse enabled" mean? Can somebody help me? Best Regards!!! Attachmentdetails.pdf (62 Downloads) |
8/23/2017 1:06 PM | |
Joined: 8/22/2013 Last visit: 6/5/2021 Posts: 62 Rating: (0) |
Dear sir, Thank you very much. |
Follow us on