Industry Online Support
Technical Forum
1/23/2024 12:30 PM | |
Joined: 1/16/2024 Last visit: 3/20/2024 Posts: 3 Rating:
|
I have the same issue and i have tried the to mentioned options (Save As with Re-organization // increase DB limit ) but the issue still repeated ("The communication resources required could not be determined for block FB5, because the block does not have an interface.") and I have tried to insert the FB5 again to generate a new instance DB but it change the instance DB Number and the issue still repeating ........do you have any idea to solve it (However the FB5 is a Impulse function and delayed On/Off(TIMR_P) ? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 01/30/2024 10:49:17New subject after splitting |
|
Follow us on