12/17/2015 8:52 AM | |
Joined: 5/12/2006 Last visit: 6/7/2024 Posts: 22255 Rating: (2986) |
Hello, have take a look in the adress overwiew in HWConfig if the Adress 90 is listed here?
Christoph |
12/17/2015 8:57 AM | |
Joined: 3/5/2013 Last visit: 6/6/2024 Posts: 71 Rating: (0) |
Hi No, It's only 27. Pls see the attached picture |
12/17/2015 9:00 AM | |
Joined: 3/5/2013 Last visit: 6/6/2024 Posts: 71 Rating: (0) |
Pls see the I 90.2 in the logic (Attached picture) |
12/17/2015 10:10 AM | |
Joined: 3/5/2013 Last visit: 6/6/2024 Posts: 71 Rating: (0) |
Please see the attached project Only CPU, IO, IM360, IM361 No HMI, 1 CPU only AttachmentU15-sootblower_a.zip (73 Downloads) |
12/18/2015 10:56 AM | |
Joined: 2/1/2011 Last visit: 9/13/2023 Posts: 186 Rating: (4) |
Dear kietnt81, Address Overview is not showing use of IB 90. As per HW configuration No GSD missing because CPU do not have DP port. Finally, as per me it can be concluded that by mistake IB 90 is used in program. |
12/20/2015 3:12 AM | |
Joined: 3/5/2013 Last visit: 6/6/2024 Posts: 71 Rating: (0) |
Thanks ashishm |
Follow us on