5/23/2024 6:52 AM | |
Joined: 12/3/2019 Last visit: 7/12/2024 Posts: 16 Rating:
|
Hey everyone, I am using a BNI PNT-508-105-Z015 IO Link module and the IO-link device connected to the master is in error mode (Undervoltage on channel no. 1). I try to use the block to debug but no success. The block keep giving me the message 15#8601 (System function WRREC reports an error, see "diagnostics"). How did you perform a module Power-cycle using the LIOLink_Device block? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 05/23/2024 08:54:36New subject after splitting Last edited by: Luh_Days at: 05/23/2024 11:14:34Last edited by: Luh_Days at: 05/24/2024 11:21:48 |
|
5/23/2024 6:54 AM | |
Joined: 12/3/2019 Last visit: 7/12/2024 Posts: 16 Rating:
|
More photos about the problem |
Last edited by: Luh_Days at: 05/23/2024 11:15:27 |
|
5/28/2024 7:43 AM | |
Joined: 12/3/2019 Last visit: 7/12/2024 Posts: 16 Rating:
|
I tried to update the post as I am trying to resolve the problem, so sorry for the amount of posts But here is the last comment that works for me: After the power-cycle, the fault persist, but a new errors in the module starting to pop-up.
You can download the GSD file on: https://www.balluff.com/sv-se/products/BNI005H Even if the version of both of the GSDs are V2.34, the gsdml-v2.34-balluff-bni-pnt-508-105-z015-20190301.xml do not work. AttachmentImages.zip (63 Downloads) |
Last edited by: Luh_Days at: 05/28/2024 07:45:16 |
|
This contribution was helpful to
1 thankful Users |
Follow us on