10/11/2023 1:47 PM | |
Joined: 10/2/2023 Last visit: 11/8/2023 Posts: 20 Rating:
|
Hi again...uf. Now I have another issue and I have been trying already 2 hours. I'll try to explain: When starting the cold heater I first must ventilate the burner room, this takes 3 minutes (B018) at full power (1000) then the feed screw brings the pellets into the burner, then the ignition heater starts and just a little after that the ventilator starts running at slow rpm's (250) until the pellets burn and the temperature sensors sees 35C (B003) when that happens the parameter value as set in my mobile should be activated as the signal/rpm's during operation. In my first program with the AI's it worked that way but somehow now with using the mathematic instruction B015 I cannot get this done. Can you please assist me on this? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 10/12/2023 08:27:59New subject after splitting |
|
10/15/2023 10:16 AM | |
Joined: 10/2/2023 Last visit: 11/8/2023 Posts: 20 Rating:
|
Hi, Now I have a strange problem. On my laptop I can change the input for the pellet feed, when changing it I get the message "submitted" below the analog value field. (VW 14) but on my phone in the browser it doesn't change when changing the value. The strange thing is that the analog value field for ventilator speed (VW16) I can change on my phone and on my laptop. The same thing happens on the phone of my son. Settings for both fields are identical (signed, writable). AttachmentInterface pellet burner 400600 resulution.zip (439 Downloads) |
10/15/2023 4:08 PM | |
Joined: 10/2/2023 Last visit: 11/8/2023 Posts: 20 Rating:
|
OK, understood. Still strange that on 1 field it works and on the other not. |
10/15/2023 4:09 PM | |
Joined: 12/18/2014 Last visit: 7/18/2024 Posts: 33374 Rating:
|
How do you leave the input fileds? With the Enter button? Or with the Tab button? |
Follow us on