11/24/2019 11:29 AM | |
Joined: 10/2/2017 Last visit: 12/8/2023 Posts: 25 Rating:
|
Hello. I was trying to use ACS450 software to connect my laptop with LMV51. I installed and registered the software on the laptop. I established the connection between AZL5 and laptop via RS232/ USB Adapter because my laptop has USB ports only. When I'm trying to connect with AZL, all efforts finish on the step of 'Reading the parameter numbers'. It can last endlessly till I stop it. I can't find the reason for this problem. Kindly find the attached screenshot below. Thanks in advance. Best regards. Hamster74. AttachmentDoc1.docx (1098 Downloads) |
Follow us on