2/15/2024 8:31 AM | |
Joined: 2/15/2024 Last visit: 4/18/2024 Posts: 29 Rating:
|
Software ver. is 8.0.0 PLC: IP: 192.168.1.15, Subnet: 255.255.255.0 PC: IP: 192.168.1.16, Subnet: 255.255.255.0 |
2/15/2024 8:37 AM | |
Joined: 12/18/2014 Last visit: 7/15/2024 Posts: 33344 Rating:
|
The IP addresses are okay. Your LOGO! is a LOGO! 8.2 and is in the hardware selection a LOGO!8.FS4. For this you need the LSC version V8.2 or higher. You can download the upgrade to LSC V8.4 from here: Download and installation instructions for LOGO! Soft Comfort Upgrade V8.4 |
2/15/2024 9:13 AM | |
Joined: 2/15/2024 Last visit: 4/18/2024 Posts: 29 Rating:
|
Thank you! Everything worked, I exported the project :> |
This contribution was helpful to
1 thankful Users |
Follow us on