2/8/2020 10:50 AM | |
Posts: 1 Rating: (0) |
Hello guys! I have a problem with the touch panel. The sensor panel doesn't work correctly I need to tune the panel. How can I DO THAT? Just when I want to select some object on the screen some times I need to touch repeatedly and some times I need to touch beside the object on the screen to select him. What can I solve this issue? Thanks ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 02/10/2020 11:28:45New subject after splitting |
|
2/8/2020 11:23 AM | |
Joined: 3/28/2015 Last visit: 10/4/2024 Posts: 721 Rating: (213) |
Hello, Perhaps the following Manual might help: SIMATIC HMI HMI devices Comfort Panels 4.3.5.6 Calibrating the touch screen Pages: 88-89 |
Eng.Mohamed Ibrahim |
|
2/9/2020 1:43 AM | |
Posts: 12 Rating: (0) |
Hello Sarvar, From Prosave, try Factory reset using MAC. If the panel is still not reachable via MAC, then you have to contact Siemens Support. Regards, Neren |
Follow us on