4/3/2013 10:33 AM | |
Posts: 247 Rating: (2) |
Hi Bilal, I want your help. i had finished the steps you mentioned in the pdf document. Now project is downloading succesfully from ES (WIndows7 Ultimate) to OS (server Windows Server 2008) and OS_standby (standby server Windows Server 2008). After downloading when trying to open from Server (OS) it is showing the error: "The user doesnot have the rights to perform this action! Please check the assignment of the current user of the user groups in windows." Even logged in user is Admin having all the security permissions which is reqiuired as per manuals. Even i had checked several manuals and help/suggessions on siemens forum and checked all the details are as per the pcs7 recommandations only. is there some thing else i have to do?? |
Last edited by: O_Moderator at: 4/4/2013 3:46 PMnew subject after splitting from /tf/WW/en/Posts/72897#top |
|
4/5/2013 2:13 PM | |
Posts: 836 Rating: (100)
|
Are you using the same username /PW settings on the ES and the target computer? Are you member in the required windows user groups? |
4/14/2013 7:11 AM | |
Posts: 247 Rating: (2) |
Hi Rugby Guy, I am using the same settings as mentioned in this documents. |
4/15/2013 11:17 AM | |
Posts: 836 Rating: (100)
|
did you try to reinstall the second server? |
This contribution was helpful to1 thankful Users |
Follow us on