Industry Online Support
Technical Forum
9/26/2011 9:38 AM | |
Posts: 4 Rating:
|
Hello. I use a IPC577C to run WinAC RTX2010 and WinCC Flex 2008 SP2 Runtime. When I press a input area on WinCC, the keypad appears after 10-20 seconds. It's like when the computer is too busy. And there is a task "S7wlpapx.exe", they use 90% od the CPU for almost nothing (http://support.automation.siemens.com/WW/view/de/34665850) I have disabled the "Preventing change of processor clockrate" option, and after few hours, no more problems with the input panel. Anybody know this problem? Any another ideas? |
12/12/2011 10:17 AM | |
Joined: 1/26/2011 Last visit: 8/11/2022 Posts: 243 Rating:
|
Hi s_oggier, can you reproduce this problem? greetings bigfoot |
7/16/2013 12:34 PM | |
Posts: 11 Rating:
|
Hello, |
Follow us on