8/31/2020 11:58 AM | |
Joined: 4/28/2015 Last visit: 4/24/2021 Posts: 6 Rating: (0) |
Hi , I am also getting the same problem . I am having the OS image version 2.1.3. When I type iot2000 setup , i am getting only 4 options and they are: OS Settings Networking Software Peripherals There is no option available in networking to configure wifi. There is no way to make a dhcp connection at wlan0 as shown in the user manuals . Need support on this . Regards, Raj ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 08/31/2020 13:55:58New subject after splitting |
|
8/31/2020 2:15 PM | |
Joined: 4/28/2015 Last visit: 4/24/2021 Posts: 6 Rating: (0) |
Please read as : Bus 001 Device 003 ID 0bda:818b Bus 001 Device 001 ID 1d6b:0002 Bus 002 Device 001 ID 1d6b:0001 |
8/31/2020 2:39 PM | |
Joined: 4/28/2015 Last visit: 8/26/2024 Posts: 3345 Rating: (379)
|
Hi,
hm, 0bda:818b stands for RTL8192EU and this is supposed to work (see this post). But you say there is no "Wifi" under Networking in iot2000setup? Best regards! |
Not working for IOT2050 support anymore from March 1st, 2024. |
|
Follow us on