11/6/2018 11:33 PM | |
Posts: 3 Rating: (0) |
Hello I have received a .s7p file which include PLC and HMI code. To open this I have been told that i need Siemens Step 7 V5.6 and WinCC V7.4 SP1. I have TIA V15 which includes Step 7 professional combo 15.0 license and WinCC Flexible Advanced 15.0. When I try to migare the project I get the following error that "There is no suitable STEP 7 version installed. Please install latest STEP 7 version." I want to know how I can open this file and migrate to TIA 15 to view the PLC and the HMI project. Thank you Bobby, ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 11/7/2018 11:58:04 AMNew subject after splitting |
|
This contribution was helpful to1 thankful Users |
11/7/2018 11:59 AM | |
Joined: 6/19/2017 Last visit: 5/24/2024 Posts: 8086 Rating: (165) |
Closed cause question posted twice. The second thread with the subject How to open file and migrate to TIA 15 to view the PLC and the HMI project? is published within the conference STEP 7 (TIA Portal).
Jen_Moderator |
My Forum is the place to personalize your profile, |
|
Follow us on