3/30/2013 6:59 PM | |
Joined: 1/28/2009 Last visit: 8/5/2024 Posts: 6844 Rating:
|
Hello , GSD contains basic configuration of a DP Slave such as permissible baud rate,number of byte of I/O to exchange with the master and other parameters.While configuring the slave in STEP7 via HW.Config.all related data stored in SDBs.Find more informationHEREand SDBs are stored in Load memory of target CPU.Also check the attachment. Best regards Hamid Hosseini AttachmentPrinting _System Data Block Numbers_.pdf (284 Downloads) |
6/26/2013 2:31 PM | |
Joined: 1/21/2013 Last visit: 6/6/2024 Posts: 4620 Rating:
|
Hi DS SURESH KUMAR, Have a look: SIMATIC PC Compact Flash - PC-based Automation - Siemens |
Follow us on