4/19/2023 11:25 AM | |
Joined: 4/15/2022 Last visit: 7/31/2024 Posts: 28 Rating: (0) |
Hi! I will go straight to the point. Is there any way of using the module 132-4BD01-0AA0 with the interface IM 151-1BA02-0AB0. I found the interface in the TIA Portal catalog but the module isn`t there. It is possible to use GSD file for the module and the interface from catalog? To mention that I already connect the interface with the CPU 1516F-3 PN/DP. Thank you! |
Follow us on