1/19/2012 10:41 AM | |
Joined: 9/23/2005 Last visit: 10/4/2024 Posts: 4349 Rating: (1446)
|
Hi, it is probably a "know feature of windows". Suggestions: First: Check if in the installation page there is a typ about how is the possible causes. Follow it. Second: take a look at FAQ http://support.automation.siemens.com/BR/view/en/8861819, it is concerning about other softwares, but once the problem comes from the windows, the probable solution is the same. |
Denilson Pegaia |
|
This contribution was helpful to2 thankful Users |
1/19/2012 11:13 AM | |
Posts: 40 Rating: (0) |
Second step FAQ worked |
1/19/2012 11:56 AM | |
Joined: 9/23/2005 Last visit: 10/4/2024 Posts: 4349 Rating: (1446)
|
I'm happy to know that. |
Denilson Pegaia |
|
1/20/2012 2:39 PM | |
Posts: 40 Rating: (0) |
hi now i can not change target directorywhen i install it just c:\..... i want to install another part
|
5/8/2014 8:10 AM | |
Posts: 340 Rating: (6) |
new question is splittet to TIA Portal V12 update to V13, uninstallation was unsuccessful |
Follow us on