12/28/2015 7:09 AM | |
Joined: 5/12/2006 Last visit: 7/25/2024 Posts: 22324 Rating:
|
Hello, here you found a overview which upload is possible: https://support.industry.siemens.com/cs/ww/en/view/97554052 But i think in you case no upload is possible because the PLC is to old. You can try to find the PLC in Accessible Nodes and show if you can access the Program Blocks, than you can try to copy the Online blocks to a project.
Christoph |
3/29/2016 4:20 PM | |
Posts: 27 Rating:
|
Hello, I am having the same problem trying to upload a TIA Portal V10.5 project from a CPU. When uploading in TIA Portal V13 an error appears saying the online module 6ES7 212-1AD30-0XB0 V1.0 does not support uploading to PG/PC, so I upgraded the firmware to V2.2.0 through an MCC card. Everything went fine, and when I go online on the CPU now it also says the online firmware version is V2.2.0. But I still get the same uploading error mentioning the V1.0 is unsupported. Screenshots are attached in a .zip Can anyone help me out with this problem? AttachmentOnline diagnostics.zip (456 Downloads) |
Last edited by: Stef_VanLoon at: 3/29/2016 4:23:47 PMLast edited by: Stef_VanLoon at: 3/29/2016 4:24:00 PM |
|
6/17/2018 7:11 AM | |
Posts: 2 Rating:
|
Hello, I am getting the following message while uploading the program in TIA portal V13. CPU model is 214-1BG31-0XB0. "Restrictions to uploading PG/PC". |
9/5/2018 1:57 PM | |
Joined: 5/12/2006 Last visit: 7/25/2024 Posts: 22324 Rating:
|
Hello, no there is no optiopn, upload not possible with this PLC.
Christoph |
Follow us on