10/2/2014 9:49 PM | |
Posts: 13 Rating:
|
Hello everyone! I apologize if this topic have already been created, but with the information that I found I could not solve my problem. I'm new in Siemens development and I hope you can help me. Here is my problem: I'm trying to exchange data between two CPUs IM151-8 PN/DP, I have already configured the GET / PUT blocks and I had created the "S7_Connection" between the CPUs. But I always get the error message 1: . Communications problems, for example . Connection description not loaded (local or remote) . Connection interrupted (for example: cable, CPU off, CP in STOP mode) . Connection to partner not yet established . Also for S7-300: . Maximum number of parallel jobs / instances exceeded. Note .: I'm simulating PLC, there is no hardware for testing. What will be the reason? In attachment I send pictures of the settings I made. From already thank you very much!
Attachmentget_put_configuration.zip (566 Downloads) |
Last edited by: Bruno Moraes at: 10/2/2014 9:55 PM |
|
This contribution was helpful to
1 thankful Users |
Follow us on