3/15/2015 10:54 AM | |
Joined: 5/7/2008 Last visit: 5/9/2024 Posts: 30 Rating: (1) |
problem hardware configuration at the attachment |
3/15/2015 10:56 AM | |
Joined: 5/7/2008 Last visit: 5/9/2024 Posts: 30 Rating: (1) |
no problem i can see watchtable analog inputs value and force analog outputs value |
3/15/2015 10:59 AM | |
Joined: 5/7/2008 Last visit: 5/9/2024 Posts: 30 Rating: (1) |
i can not find where is the problem.urgently |
3/15/2015 6:55 PM | |
Posts: 784 Rating: (52) |
Hello, You simulate peripheral addressing in TIA Portal by adding :P at the end of the variable. Best regards......... |
6/23/2016 9:14 AM | |
Joined: 4/28/2015 Last visit: 2/7/2024 Posts: 10533 Rating: (819) |
Hello, look to this topic: |
With best regards... |
|
Follow us on