3/12/2024 6:00 AM | |
Joined: 3/11/2019 Last visit: 8/20/2024 Posts: 1555 Rating:
|
Hi, "TCON_IP_V4" can be directly used as data type of a tag. For example in a data block or in the static of an FB. You have to type this manually (complete). It will work. This tag can be connected to the parameter. Its also shown in this FAQ: How do you program and parameterize Modbus/TCP communication between S7-1500 CPUs and S7-1200 CPUs?-> net_modbus_tcp_s7-1500_s7-1200_en.pdf (1,0 MB) -> picture 3-3 page 15 regards sancruz |
Last edited by: sancruz at: 03/12/2024 06:01:31Feedback appreciated, please rate |
|
This contribution was helpful to
1 thankful Users |
3/12/2024 12:39 PM | |
Joined: 3/12/2024 Last visit: 5/23/2024 Posts: 12 Rating:
|
>For example in a data block or in the static of an FB. This is what I was missing. Thank you. |
Follow us on