7/23/2024 7:57 AM | |
Joined: 1/21/2013 Last visit: 7/25/2024 Posts: 3019 Rating:
|
Hi MSKehribar, This is an international and English-speaking forum, so please keep that in mind when posting.
To configure a WinCC Unified device, the WinCC Unified engineering software must be installed. This is not installed by default and may be blocked by other software already installed. You should try to run the setup for STEP 7 and WinCC Unified again and select WinCC Unified. If it cannot be selected, the message that appears will tell you more about the current restriction. For further assistance, please refer to the list of installed SIMATIC software from the TIA Portal. Kind regards |
7/24/2024 11:07 AM | |
Joined: 1/21/2013 Last visit: 7/25/2024 Posts: 3019 Rating:
|
Hi MSKehribar, It is not the licenses that prevent you from using WinCC Unified. When installing STEP 7 and WinCC you have to select WinCC Unified yourself, it is not pre-selected. You should start the setup routine again and select WinCC Unified for installation. If you also want to be able to simulate the panel on your PC, you must also install WinCC Unified PC Runtime. However, this may be prevented by the installed WinCC Professional Runtime. Kind regards |
Follow us on