6/3/2017 10:05 AM | |
Joined: 9/30/2016 Last visit: 8/15/2024 Posts: 914 Rating: (6) |
After cleaning up as previously posted I just tried again. I started with SIMATIC STEP 7 Professional V13.0 SP2 and it seemed to install without errors. As far as I can read it is not possible to download a WinCC Anvanced for V13.0 SP2 anymore so that must be handled by V14 SP1 - is that correct ? Then I tried to install SIMATIC_S7_PLCSIM_V13_00_02_00 but it ended with errors - see attached error report. What does this/these errors mean and how do I fix it ? I will now uninstall / clean up again and try to start with V14 SP1 - I hope I can install V13 SP2 afterwards (if I am successful )? AttachmentSIA_S7-PLCSIM_V13_SP2@17-06-03_08-12-17_summary.zip (313 Downloads) |
Last edited by: xmnj at: 6/3/2017 10:07:00 AM |
|
6/4/2017 11:39 AM | |
Joined: 5/12/2006 Last visit: 8/14/2024 Posts: 22343 Rating: (3003)
|
Hello, WinCC Advanced V13 SP2 can be downloaded here:
This often happen if a Antivurs SW is blocking the files, have you disabled/uninstalled the AntivursSW before you try to install the SW? Christoph |
This contribution was helpful to1 thankful Users |
6/6/2017 7:57 AM | |
Joined: 9/30/2016 Last visit: 8/15/2024 Posts: 914 Rating: (6) |
Hi again, Thank you to ChristophD and huggy_d1. I did find the SP2 files - thanks - I should have posted that. I have not disabled the AV - but I am getting closer. I THINK the main problem was that I did not start the installation files with "run as Administrator". As always please see attached screenshots and crash dumps. Now I CAN open the project view and move around in the files. It makes a crash when I close the TIA Portal (see first crash dump) - that would be tolerable. What is not possible to work with is that it also crashes when I try to start a simulation of the HMI (MON) (see second crash dump). I managed (as administrator) to install all of the program parts with the exception of SIMATIC TIAP V14.0 SP1 Upd1 and a small Sinamics update (HSP0185). For some reason the SP1 Upd1 package will not install. I have tried directly from the downloaded file and via the TIA Updater (and now the installed says it cannot be removed either). The HSP0185 I have not dared trying to install since it seemed that the failed installation of that one was was made the crashing start in the first place. What is the next step in getting my TIA SW work ?
Attachmentcrash7.zip (272 Downloads) |
8/30/2017 10:27 AM | |
Joined: 8/21/2014 Last visit: 8/15/2024 Posts: 1006 Rating: (13) |
New question published by samiraj is split to a separate thread with the subject I can't download this file SIMATIC_STEP_7 file even i have done registration. Best regards |
My Forum is the place to personalize your profile, |
|
Follow us on