9/28/2017 11:25 AM | |
Joined: 11/16/2016 Last visit: 11/20/2024 Posts: 45 Rating: (1) |
I have Tia portal V13 sp1 and when I want to connect and download a program to a plc (S7-1200)the connection is not posible. I see the IP of the plc and I can flash the LED but I can not download the program to PLC. I'm sure that my network card of pc work properly and the cable was good also and the plc too because I can connect withe an other pc but not with mine, knowing that I searche a solution of this problem in this forum but I don't find it, knowing that I don't have an anti-virus and I désactivate a firewall of windows7. you find enclosed the photo of the error code What can be the problem ? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 9/28/2017 12:39:40 PMNew subject after splitting |
|
12/24/2017 3:55 PM | |
Joined: 11/16/2016 Last visit: 11/20/2024 Posts: 45 Rating: (1) |
I activated the PUT / GET but the problem persists |
12/24/2017 4:36 PM | |
Joined: 4/28/2015 Last visit: 1/10/2025 Posts: 10733 Rating: (834)
|
Hello, which TIA SW Update? You've mentioned only SP1. |
With best regards... |
|
12/24/2017 6:01 PM | |
Joined: 2/6/2015 Last visit: 1/11/2025 Posts: 61 Rating: (19) |
Hi, The IP address detected by TIA Portal is 147.91.9.41. The IP Address you have mentioned are in very different range. Can you set the IP in same range as PLC? Maybe, WireShark or Microsoft Network Manager will assist you better in finding Network Issues. Best Regards Kaushal Joshi |
Kaushal Kumar Joshi |
|
12/25/2017 8:13 AM | |
Joined: 5/8/2016 Last visit: 2/15/2024 Posts: 167 Rating: (13) |
hey 1- check the part number and version of the CPU , maybe the version is not supported by tia v13 sp1 2- try to make the ip of your device in the same domain of the PLC , or make it automatic and try again . 3- If the CPU used before maybe its write protected , so if you don't need to the program in the CPU format it, that will help . regards ahmed hamad |
A lot of potential remains |
|
Follow us on