6/19/2015 9:44 AM | |
Joined: 10/24/2013 Last visit: 5/9/2024 Posts: 11 Rating:
|
I have got similar problem with TIA V13 SP1 to Windows 7-64bit. Even I was able to connect to a CPU s7-1212 or to as7-1215, to drive to Start or Stop, to Download or Upload, to Change PROPERTIES and IPs, in "Accecible notes" found nothing at all. I tried and the primary setup tool and nothing.The maximum problem will come when I try to connect with NEW one CPU with no or Unknown IP. A week ago i were able to communicate perfectally with same CPUs, same etrernet cords, same Pci cart, same Project in TIA v11 with Windows XP.I re-instalated the TIA, the Driver of ethernet cart,All setings were OK, all diagnostics were OK, but "no accecible note in network". (the pci-cart was work ok, I had Internet and local network by other PCs). After too many tests, advices,I thought to try another Pci cart. I installed and -miracle- all are OK!!!!!!!
---------------------------------------------------------------------------------------------------- |
Last edited by: Min_Moderator at: 6/19/2015 1:56:33 PMNew subject after splitting |
|
6/19/2015 1:57 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4767 Rating:
|
|
Follow us on