12/14/2015 1:51 PM | |
Posts: 5225 Rating: (1189)
|
Which TIA Portal components do you have installed? (Step7, WinCC,..) You could try to get the files from.... https://support.industry.siemens.com/cs/document/109311724/ |
12/14/2015 1:51 PM | |
Joined: 5/12/2006 Last visit: 7/25/2024 Posts: 22324 Rating: (2999)
|
Hello, run the UPD6 setup again. Alternativ: Download the UPD6 installdata from the Web and install it. https://support.industry.siemens.com/cs/ww/en/view/109311724 Regards Christoph |
12/14/2015 2:05 PM | |
Posts: 4 Rating: (0) |
The "old" STEP 7 V5.5 is working fine! |
12/14/2015 2:10 PM | |
Posts: 4 Rating: (0) |
Okay, try that Thanks |
12/14/2015 2:36 PM | |
Joined: 7/9/2015 Last visit: 7/25/2024 Posts: 3892 Rating: (571) |
Hi,
yes, perhaps it´s better to install complete new. Here´s a FAQ how to deinstall TIA complete. https://support.industry.siemens.com/cs/de/en/view/76325723 Siemens advises to disable the antivirus software during installation...perhaps one reason for the crash?
If you are using and have installed STEP 7 Safety, please note that, in addition to the TIA Portal Update 6, at least the installation of STEP 7 Safety Update 4 is also essential. Updates for STEP 7 V13 SP1 and WinCC V13 SP1 https://support.industry.siemens.com/cs/de/en/view/109311724
Regards, Towome
|
|
|
1/15/2016 12:09 AM | |
Posts: 61 Rating: (1) |
I have a similar but different error. see pic Is there no option other than to uninstall TIA completely ?
|
Follow us on