2/18/2020 7:23 PM | |
Joined: 5/27/2014 Last visit: 10/26/2022 Posts: 109 Rating: (6) |
Hello, I have TIA V15.1 install on my computer (Windows 7 Professional, also TIA V13 is installed) and I'm trying to install update 4 from this link https://support.industry.siemens.com/cs/pe/en/view/109763890 , but instalation fails with following log. I tried to reboot the computer, run installation as an administrator, run the installation from external drive, but always the same result. Any ideas what's wrong? OS: Microsoft Windows 7 Professional Professional, Service Pack 1, 64-bit, build 7601 COMMANDLINE: C:\Program Files (x86)\Common Files\Siemens\Automation\Siemens Installer Assistant\407\SIA2.exe /l1033 /starter /bundlepath=C:\SIMATIC TIAP V15.1 UPD4\InstData INSTALLDIR: C:\Program Files\Siemens\Automation SETUPLANGUAGE: 1033 PRODUCTLANGUAGES: 1033 CHANGES: (+)Automation Software Updater;(+)TIACOMPCHECK;(+)PE_Upd;(+)SIMATIC_Upd;(+)IECPL_Upd;(+)HM_AllEditions_Upd;(+)HM_NoBasic_Upd;(+)ES_Upd;(+)WinCC_TR_Mandatory_Upd;(+)WinCC_TrC_All_Upd;(+)WinCC_TrC_CAP_Upd;(+)Start_Sicman;(+)HMIRTMV11_Upd;(+)RT_Adv_SIM_Upd There are NO severe messages before the installation 19:13:54 | BEGIN. Execution started. 19:13:56 | OK RunningProcesses () Complete 19:13:56 | OK InventoryBefore (A) Complete 19:13:56 | OK Citamis (Before) Complete 19:13:57 | OK SecurityControlFeature (ReturnFeatures) Complete 19:13:57 | OK ClassicCompPrepare () Complete 19:13:58 | OK ProductRegistration (Before) Complete 19:13:58 | OK ClassicCompAfterUninstall () Complete 19:14:02 |ERROR AdsWorkerClassicComponent::OnWorkerCompleted(): - ClassicProduct setup failed due to unknown error 19:14:02 | FAIL! SetupUnit (Automation Software Updater)Failed ClassicComponentAddLocal 19:14:06 | OK SetupUnit (TIACOMPCHECK) Complete Foreign AddLocal 19:14:06 | SKIP! SetupUnit (PE_Upd) Skip Patch AddLocal 19:14:06 | SKIP! SetupUnit (SIMATIC_Upd) Skip Patch AddLocal 19:14:06 | SKIP! SetupUnit (IECPL_Upd) Skip Patch AddLocal 19:14:06 | SKIP! SetupUnit (HM_AllEditions_Upd) Skip Patch AddLocal 19:14:06 | SKIP! SetupUnit (HM_NoBasic_Upd) Skip Patch AddLocal 19:14:06 | SKIP! SetupUnit (ES_Upd) Skip Patch AddLocal 19:14:06 | SKIP! SetupUnit (WinCC_TR_Mandatory_Upd) Skip Patch AddLocal 19:14:06 | SKIP! SetupUnit (WinCC_TrC_All_Upd) Skip Patch AddLocal 19:14:06 | SKIP! SetupUnit (WinCC_TrC_CAP_Upd) Skip Patch AddLocal 19:14:10 | OK SetupUnit (Start_Sicman) Complete Foreign AddLocal 19:14:10 | SKIP! SetupUnit (HMIRTMV11_Upd) Skip Patch AddLocal 19:14:10 | SKIP! SetupUnit (RT_Adv_SIM_Upd) Skip Patch AddLocal 19:14:10 | OK ClassicCompAfterInstall () Complete 19:14:10 | OK ClassicCompRollback () Complete 19:14:10 |ERROR HspInstallWorker::ApplyUpdates(): - Applying patches failed with return code: ERROR_INSTALL_SOURCE_ABSENT 19:14:10 |ERROR HspInstallWorker::ApplyUpdates(): - Applying patches failed with return code: ERROR_INSTALL_SOURCE_ABSENT 19:14:10 |ERROR HspInstallWorker::ApplyUpdates(): - Applying patches failed with return code: ERROR_INSTALL_SOURCE_ABSENT 19:14:10 |ERROR HspInstallWorker::ApplyUpdates(): - Applying patches failed with return code: ERROR_INSTALL_SOURCE_ABSENT 19:14:10 |ERROR HspInstallWorker::ApplyUpdates(): - Applying patches failed with return code: ERROR_INSTALL_SOURCE_ABSENT 19:14:10 |ERROR HspInstallWorker::ApplyUpdates(): - Applying patches failed with return code: ERROR_INSTALL_SOURCE_ABSENT 19:14:10 |ERROR HspInstallWorker::ApplyUpdates(): - Applying patches failed with return code: ERROR_INSTALL_SOURCE_ABSENT 19:14:10 | OK HspInstall () Complete 19:14:11 | OK MspInstall () Complete 19:14:21 | OK ProductRegistration (After) Complete 19:14:31 | OK SetupIsComplete () Complete 19:14:32 | OK InventoryAfter (Z) Complete 19:14:32 | OK LicenseTransfer (True) BeforeStart 19:14:32 | OK Citamis (After) Complete 19:14:33 | OK SetupSummary () Complete 19:15:06 | OK SetupReport () Complete 19:15:06 | END. Execution completed. Intermediate ExitCode after execution queue : 1603 - Exit code means: Installation failed ( ) Errors: 8 Warnings: 0 |
Last edited by: Petr Broza at: 02/18/2020 19:24:45Last edited by: Jen_Moderator at: 02/19/2020 12:28:25Optimized link. TIA V16 update 4, STEP 7 Professional+safety |
|
4/6/2020 12:23 PM | |
Joined: 12/2/2010 Last visit: 6/19/2024 Posts: 25 Rating: (1) |
Have you fix the problem ? If yes, How did you proceed ? |
4/14/2021 4:01 PM | |
Posts: 1 Rating: (0) |
|
Follow us on