1/4/2022 7:30 PM | |
Posts: 257 Rating:
|
Hello SIOS Forum Community, We are receiving more and more enquiries about which new S7-1500 hardware will be released with which quantity structure under TIA V17. Here is a selection: - CPU 1518HF-4 PN (6ES7518-4JP00-0AB0), the new innovative SIMATIC S7-1500H CPU with integrated F-functionality - predestined for applications that have both high availability and fault tolerance requirements. - CPU 1518T(F)-4 PN/DP (6ES7518-4UP00-0AB0), the high-end S7-1500 technology CPU for demanding motion control applications with very high requirements in terms of program scope, networking and processing speed. The CPU with a quantity structure of up to 192 axes is available without and with integrated error protection. - CPU 1518 with an extended memory quantity structure: The working memory of the CPUs 1518 (including T, F, TF, HF) is significantly expanded. - For CPUs 1517 and 1518, the number of UDP multicast circuits has been expanded. - For CPUs 1510SP to 1513 (including CPU 1513R) and CPU 1515 (including CPU 1515R), the quantity structure has been increased with regard to the number of modules (and UDTs). - TM MFP (Technology Module Multifunctional Platform), this module is predestined for IT applications in automation technology, i.e. for applications that directly evaluate and process data and information from the CPU, but are not directly involved in the actual control task. The current quantity structure of the respective CPU is documented in the technical data, which can be found at SIOS. Further information can be found here in the forum on the TIA V17 delivery release and in the SIOS in the Step 7 V17 manual. Best regards, SIMATIC International Technical Support Hub. |
Last edited by: SIMATIC International Technical Support Hub at: 01/04/2022 20:43:20 |
|
This contribution was helpful to
1 thankful Users |
Follow us on