Industry Online Support
Technical Forum
8/2/2011 2:08 PM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181) |
Hello, Yes, you can use SFB4 more then once in software. And the max. duration of it is 24d:20h:31min:23sec:647ms And take a look at http://support.automation.siemens.com/WW/view/en/18723826 Best regards, Hristo Mihalev |
Last edited by: UMENCHO at: 8/2/2011 2:25 PMtypo Last edited by: UMENCHO at: 8/2/2011 2:24 PMLast edited by: UMENCHO at: 8/2/2011 2:16 PM |
|
This contribution was helpful to1 thankful Users |
8/2/2011 2:26 PM | |
Joined: 1/28/2009 Last visit: 4/26/2024 Posts: 6838 Rating: (1359) |
SFC4 versus SFB4, check the attachment! Also check the following threads for more points: Why is TON made as FB?TOTAL TIME IN HH/MM/SS FORMAT (HOUR/MINUTE/SECOND)Best regards AttachmentSFB4 VS SFC4.zip (76 Downloads) |
Last edited by: hdhosseini at: 8/2/2011 2:46 PM//links added |
|
This contribution was helpful to2 thankful Users |
Follow us on