Industry Online Support
Technical Forum
8/28/2009 4:02 AM | |
Posts: 24 Rating: (1) |
Dear Tomazb, The op/ktp/device you are using have not inbulit battery/capacitor which stores the time when power cuts from the device.but there is also another posibility by which you can correct your problem.may be you have an idea of Area Pointer in winccflexible project, there you have to specify the plc date/time tag and then you done..every thing works well. actually with above method your device try to synchronice its Date/time with the controller by which its is connected. herein attachment i will send you one simatic manager project(developed in v5.4) which has integrated winccflexible project(developed in 2008sp1 version). hope it would solve your problem. AttachmentTp177a_Time_Sync.zip (132 Downloads) |
8/28/2009 7:03 AM | |
Posts: 4 Rating: (0) |
thank you! |