1/7/2012 5:44 PM | |
Posts: 140 Rating: (0) |
I have attached the my function that is calculating period of a signal waveform over like 120 seconds and then output the average period of a cycle over 120s time interval.
AttachmentFB71.pdf (178 Downloads) |
1/7/2012 5:45 PM | |
Posts: 140 Rating: (0) |
I have attached another function that is outputting the period of signal after each complete cycle. Please suggest how can I do the above two scenarios when there is no zero crossings. Hope now you have a clearer picture of what I intend to achieve. Thanks!
AttachmentFB72.pdf (161 Downloads) |
1/7/2012 6:41 PM | |||||||||||||||||
Joined: 1/28/2009 Last visit: 4/26/2024 Posts: 6838 Rating: (1359)
|
DearKhyzer, You can think about using hardware solutions such as: Frequency/Pulse Conversion
Best regards, Hamid Hosseini
|
||||||||||||||||
Follow us on