8/27/2013 11:32 PM | |||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
Joined: 1/23/2013 Last visit: 10/17/2024 Posts: 38 Rating:
|
Dear Sirs! We have PCS7 V8.0 UPD1 system configured with several AS with ET200M configured for "High-precision time stamping with 1 ms accuracy" as described in manuals of PCS7. We are facing problem that we receive to alarms to OS like:
We use Siemens clock TC100, S7-400 with CPU416-2, dual optical ring with scalance ethernet switchs. Simatic clock TC100 is configured as "Simatic time", same also for AS station. AS send time to DP in 1s intervals. CPU load is about 75% As far I understand manual this messages (in manual described as "Time difference between the messageframe time stamp and the real-time clock may cause inaccuracy") come in pair and tells: - "comming" message with time before time synchronization - "going" message with time after time synchronization In our case time is each minute corrected 2 times for a difference about 20-35ms. Shouldn't this messagesmore rarely? Any idea what could be wrong? In another test we change to 10s period of sending time to DP and messages arrivedmore rarely, but also a lot of them. This problem is further notifiend in another problem of receiving changes(messages of EVENT_TS) of digital input to OS.
Attachmentarchitecture.pdf (162 Downloads) |
||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
2/9/2017 8:42 AM | |
Joined: 1/23/2013 Last visit: 10/17/2024 Posts: 38 Rating:
|
We didn't use SIMATIC time as time synchronization source. We use NTP. BR JP |
3/10/2021 6:39 AM | |
Joined: 9/1/2017 Last visit: 2/3/2025 Posts: 156 Rating:
|
Hi
Anyway if your plant bus synchronized in simatic mode you can define your os servers as cooperative time master incase of losing central time master(siclock for example). Regards Hosein
Attachmentps7tsy_b_en-US (1).pdf (115 Downloads) |
Follow us on