2/19/2020 1:11 PM | |
Posts: 2 Rating: (0) |
Hi all, I am trying to time sync a comfort panel (running Windows CE) with a PC. I am using NTP. When I insert the server name, it auto-populates the IP address but the NTP request always times out. I have managed to time sync the HMI project using area pointers (this has nothing to do with the OS so please don't recommend this). Please advise. AttachmentDoc1.pdf (167 Downloads) |
2/20/2020 5:39 AM | |
Joined: 7/5/2013 Last visit: 11/13/2024 Posts: 3120 Rating: (516) |
Hello Ghost, the PC is configured as NTP server and the service is running? How do you configure your PC as NTP server? Regards, Frink |
Pi is exactly three! |
|
2/20/2020 11:21 AM | |
Posts: 2 Rating: (0) |
Yes all is setup correctly on the PC. |
Follow us on