8/7/2019 2:16 PM | |
Joined: 8/3/2009 Last visit: 6/5/2024 Posts: 12991 Rating: (1655)
|
Hello With which PLCs do you use the Comfort Panels? If you use for example S71500 PLCs then I would use the NTP Sxnchonisation from the Time Master to the S71500 PLc s and the PLCs are Masters for the Panels. This is the best way, because the Comfort Panels cannot perform a autmoatically Summer/Wintertime Change by their own. the need always a PLC to do it: -< LINK Like This: PC with NTP MAster ->(NTP) -> PLC->(S7Channel as Slave) -> HMI Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on