3/27/2017 10:28 AM | |
Joined: 1/6/2009 Last visit: 7/8/2024 Posts: 134 Rating: (2) |
Hello I'm having a similar problem with summer and winter time synchronization. I'm doing time synchronization with a CP 6GK7 343-1CX10-0XE0 v3.0 which works fine with time but don't update local time to summer and winter time. Can someone give me a help? ------------------------------------------------------------------------------------------ |
Last edited by: nunobnk at: 3/27/2017 10:28:51 AMLast edited by: Min_Moderator at: 3/28/2017 11:52:04 AMNew subject after splitting |
|
3/27/2017 10:38 AM | |
Joined: 8/3/2009 Last visit: 9/18/2024 Posts: 13728 Rating: (1728) |
Hello if you use NTP for time synchronisation then the automatically summer/winter time switch is not defined. so you have to use Blocks in your PLC Program for this. (is written in System Manual of the CP) like: https://support.industry.siemens.com/cs/ww/en/view/19324378 Bye Murof |
If this Information really helps, you could use the Rate function |
|
3/27/2017 11:37 AM | |
Joined: 1/6/2009 Last visit: 7/8/2024 Posts: 134 Rating: (2) |
Hello Murof, But in my case how I can synchronise the PLC clock to summer and winter time? Do exist some function to write the PLC clock after get time from PLC and use BL_LT? Thank you for your help. |
Follow us on