Industry Online Support
Technical Forum
12/6/2011 7:31 AM | |
Posts: 557 Rating: (64) |
Hi, I am using winCC with other controller, need time synconization. Pls guide to write script on it. Regards |
12/6/2011 7:44 AM | |
Joined: 10/3/2010 Last visit: 4/25/2024 Posts: 1552 Rating: (188) |
What other controller? Which communication link between WinCC & other controller? Should WinCC write its time to the other controller or other controller writes to WinCC? Can other controller read WinCC tags? ... ... ... With this little info, I don't think anyone can help you. |
B r g d s , |
|
12/6/2011 8:20 AM | |
Posts: 557 Rating: (64) |
Hi, It is Legacy LC300. it is commucating with WinCC. We can create tags also.. I need to know the script in WinCC which can synconize the format. Regards |
12/7/2011 10:02 AM | |
Posts: 1776 Rating: (95)
|
Hi, maybe this FAQ can help you. http://support.automation.siemens.com/WW/view/en/26730928 |
Follow us on